技術ウェビナー&セミナー
専門家と話そう
技術ウェビナー&セミナー Semikron Danfoss
パワーエレクトロニクスメーカーとしてのSemikron Danfossは、お客様や関係者との技術的な対話を大事にしています
技術ウェビナーに参加する
プロダクトマネージャーやアプリケーションエンジニアを含む当社の専門家が、幅広いアプリケーション向けのパワーエレクトロニクスのトピックをご紹介いたします。最後に質疑応答があります。
テクニカルセミナーおよびワークショップに参加する
詳細なディスカッションを目的としたテクニカルセミナーとワークショップは、特定のお客様グループ向けの特別なトピック、または個別のお客様との特定のプロジェクトに関するディスカッションに焦点を当てています。
過去に開催したセミナー
SKiiP 4 SiC: The First SiC Intelligent Power Module for 1500VDC Applications
The well-established SKiiP family will soon be joined by the first silicon carbide IPM. SKiiP 4 SiC enables high-power converters for Solar and ESS, Green Hydrogen and more with lower overall costs.
Join our webinar March 19th at 16:00 CET.
SKiiP 7: Latest Generation Intelligent Power Module for Drives and Beyond
The newest member of the well-established SKiiP IPM family is here. The SKiiP 7 enables customers to design converters with higher power density or reduced cost per unit area.
Join us on November 15 at 16:00 CET to see all the features.
Silicon Carbide in AC Motor Drives
Silicon carbide has increased the efficiency of power converters in many applications. However, general purpose motor drives have not been able to benefit from SiC due to cost and technical limitations. Now, changing market conditions and advances in technology mean SiC makes sense in variable torque applications. When considering the complete motor drive, the return on investment for SiC becomes apparent. Equally important is understanding the reliability of this high-performance technology.
Please join us on June 13 at 16:00 CEST to learn how SiC is a now a cost-effective and reliable solution.
Benefits of Schottky Barrier Diodes
In recent years, silicon carbide Schottky barrier diodes are increasingly used in high power applications. These devices differ fundamentally from traditional silicon pn diodes. This webinar explains the behaviour differences and how to take advantage of these differences in a converter.
Power Module Reliability: Humidity
High humidity environments present a relatively common, but not well understood, problem for power electronics. Properly addressing seemingly random humidity-induced failures requires an understanding both of the environment around a power semiconductor module as well as the high-risk operating conditions. If you work on the design or field service of outdoor power electronics systems, please join us on July 26, 2022 at 16:00 CEST.